Products
General information
- Surge protection:
Power supply: Red/Line
IT networks: Yellow/Line
- Lightning protection/Earthing
- Safety equipment
Lightning protection - more important than ever!
"External lightning protection" protects buildings against destruction
by lightning.
In Germany, lightning strikes two times per square kilometre
every year - this leads to serious damage.
Lightning
protection means more than just a Faraday Cage of air terminations,
down conductors and an earthing system.
Also the electromagnetic effects of lightning have to be taken into consideration
and, if possible, a shielding of the building has to be installed. For a modern
lightning protection, all available metal parts of the structure are therefore
used for conducting the lightning currents to earth. For steel-structure
and reinforced-concrete buildings, the supports for the steel structure or
the steel reinforcement are connected with the down conductors. Special terminals
have been developed for connecting the steel reinforcements and fixed earthing
terminals. Roof superstructures are no longer connected directly with the air-termination. Air-termination rods or air-termination frameworks prevent a direct
lightning strike.
As a module system, the DEHNiso product family allows a simple application.
When installing the earthing system, the specific earth resistance of the ground
has to be taken into consideration. This applies to all types of earth electrodes,
even for foundation earth electrodes in accordance with DIN 18014. These are
normally used as lightning protection earth electrodes, if corresponding terminal
lugs and points are led out of the foundation. It has to be observed that terminal
lugs or points are protected against corrosion. Conductor material with a plastic
coating or high-alloyed stainless steel (V4A) comes up to this requirement.
The installation of a lightning protection system has to be performed by a
lightning protection expert or under his supervision.
An obligatory part of a lightning protection system is the lightning protection
equipotential bonding, also called internal lightning protection.
DEHN + SÖHNE offers components and equipment for complete lightning
protection systems in accordance with all applicable standards.