Company profile / Environment
Careful treatment of resources
Careful treatment of resources will, in the long run, lead to economic advantages...
... and consequently also to advantages for our customers!
Certification according to DIN EN ISO 14001
Since November 2000 our environmental management system has been certified according to DIN EN ISO 14001. Moreover, we participate in the "Umweltpakt Bayern" (Bavarian Environmental Agreement).
This certificate is only valid for a limited period of time. Annual inspections and a complete re-audit every three years ensure that "environmental issues" are always a major concern for our company.

If you require the environmental certificate, please send an email to Umweltzertifikate@dehn.de
Protection of the environment is an important topic for us
Our activities in detail:
- Utilisation of waste heat:
Waste heat deriving from production is used for heating.
- Recycling:
Plastic waste is collected and recycled. - Latest environmental technology:
A solar system as well as a rainwater utilisation system help to preserve resources. - Efficient energy input:
The consumption of electrical energy is reduced due to our energy management system.
- Waste:
Waste is sorted into special containers located in the production area
- Reliability:
Special training as well as specific regulations make our employees feel responsible for the protection of the environment in their scope of duties.
- Supervision:
Environment-related installations and activities are systematically controlled by schedules, cadasters and balances.
- Re-circulation systems:
The cooling water of our production machines is kept in a closed
re-circulation system.
- Surface water recycling:
Rain water is led back into the ground via our soaking pit.
- Safe waste storage:
Waste is safely stored in the waste storage centre until it is properly disposed of.
- Ventilation systems:
Our soldering work stations are equipped with modern ventilation systems.
- Sealed cleaning systems:
Hermetically sealed cleaning systems are used for cleaning special components.
- Thorough check of incoming goods:
Environmentally relevant goods are checked on arrival.
- Measures to save water:
Water-saving measures have been installed in our surface treatment systems. Moreover, the necessary energy resources are permanently controlled and documented.
- Vehicle fleet:
Vehicles and system components are cleaned at our special washing site. A filtering system separates the oil. We therefore select our vehicles, taking into account ecological aspects.
- Lubricants and oil:
Lubricants for cooling and hydraulic oils are controlled and cleaned for longer use